LTE TDD
For Waveform Playback (ARB) capability.
This topic describes the settings of the Downlink > Sync Signals node for an Advanced TDD Downlink carrier.
P-SS/S-SS Transmit Antenna Port
Turns the Primary Synchronization Signal (PSS) On or Off.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS[:STATe] ON|OFF|1|0 [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS[:STATe]? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS[:STATe] ON :RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS[:STATe]? |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the power level, in dB for the primary synchronization signal, relative to the average subcarrier power.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS:POWer <rel_ampl> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS:POWer? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS:POWer 0 :RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS:POWer? |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
-60 |
|
Max |
20 |
|
Initial S/W Revision |
A.20.01 |
Turns the Secondary Synchronization Signal (SSS) On or Off.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SSS[:STATe] ON|OFF|1|0 [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SSS[:STATe]? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:CCARrier:DLINk:SSS[:STATe] ON :RADio:LTETdd:WAVeform:CCARrier:DLINk:SSS[:STATe]? |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |
Sets the power level, in dB for the secondary synchronization signal, relative to the average subcarrier power.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SSS:POWer <rel_ampl> [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SSS:POWer? |
|
SCPI Example |
:RADio:LTETdd:WAVeform:CCARrier:DLINk:SSS:POWer 0 :RADio:LTETdd:WAVeform:CCARrier:DLINk:SSS:POWer? |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
-60 |
|
Max |
20 |
|
Initial S/W Revision |
A.20.01 |
Selects the P-SS/S-SS Transmit Antenna Port type.
This setting specifies the antenna port(s) that P-SS and S-SS are transmitted on. P-SS and S-SS can be transmitted on a single antenna (Port 0/1/2/3) or all antenna ports.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS:ANTenna:PORT P0|P1|P2|P3|ALLPort [:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PSS:ANTenna:PORT? |
|
SCPI Example |
RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS:ANTenna:PORT ALLPort RADio:LTETdd:WAVeform:CCARrier:DLINk:PSS:ANTenna:PORT? |
|
Couplings |
This setting is coupled to Total Number of Antenna.
|
|
Preset |
P0 |
|
State Saved |
Yes |
|
Min |
N/A |
|
Max |
N/A |
|
Initial S/W Revision |
A.20.01 |